Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ZAxisSmoothing.Options |
ZAxisSmoothing.Options.NONE
none
|
static ZAxisSmoothing.Options |
ZAxisSmoothing.Options.ON
on
|
Modifier and Type | Method and Description |
---|---|
ZAxisSmoothing.Options |
ZAxisSmoothing.option()
Returns the z axis smoothing option.
|
static ZAxisSmoothing.Options |
ZAxisSmoothing.Options.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ZAxisSmoothing.Options |
ZAxisSmoothing.Options.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ZAxisSmoothing.Options[] |
ZAxisSmoothing.Options.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ZAxisSmoothing.setOption(ZAxisSmoothing.Options option)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.