Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
WireGuide |
WireTool.createWireGuide()
Create a wire guide
License requirements: cam_base ("CAM BASE") . |
WireGuide |
WireGuideList.findItem(int index)
Returns the object at the input index.
|
WireGuide[] |
WireGuideList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
WireGuideList.append(WireGuide object)
Appends an object to the list
License requirements: None. |
void |
WireGuideList.append(WireGuide[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
WireGuideList.erase(WireGuide obj)
Erases the object from the list, but does not delete the object.
|
void |
WireGuideList.erase(WireGuide obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
WireGuideList.findIndex(WireGuide obj)
Finds the index where the input object appears.
|
void |
WireGuideList.insert(int location,
WireGuide object)
Inserts an object at the specified location
License requirements: None. |
void |
WireGuideList.setContents(WireGuide[] objects)
Sets the contents of the entire list.
|
void |
WireGuideList.swap(WireGuide object1,
WireGuide object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.