Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.BackburnPassesTypes.MULTIPLE_CUTOFF_FIRST
multiple backburn passes - cutoff first
|
static WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.BackburnPassesTypes.MULTIPLE_REGION_FIRST
multiple backburn passes - region first
|
static WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.BackburnPassesTypes.SINGLE
single backburn pass
|
Modifier and Type | Method and Description |
---|---|
WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.backburnPasses()
Returns the Backburn Passes
License requirements: cam_base ("CAM BASE") . |
static WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.BackburnPassesTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmOperationBuilder.BackburnPassesTypes |
WedmOperationBuilder.BackburnPassesTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmOperationBuilder.BackburnPassesTypes[] |
WedmOperationBuilder.BackburnPassesTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmOperationBuilder.setBackburnPasses(WedmOperationBuilder.BackburnPassesTypes backburnPasses)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.