Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmGeomBuilder.StopPointFlagTypes |
WedmGeomBuilder.StopPointFlagTypes.NONE
stop point option none
|
static WedmGeomBuilder.StopPointFlagTypes |
WedmGeomBuilder.StopPointFlagTypes.SPECIFY
stop point option specify
|
Modifier and Type | Method and Description |
---|---|
WedmGeomBuilder.StopPointFlagTypes |
WedmGeomBuilder.stopPointFlag()
Returns the Stop Point Flag
License requirements: cam_base ("CAM BASE") . |
static WedmGeomBuilder.StopPointFlagTypes |
WedmGeomBuilder.StopPointFlagTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmGeomBuilder.StopPointFlagTypes |
WedmGeomBuilder.StopPointFlagTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmGeomBuilder.StopPointFlagTypes[] |
WedmGeomBuilder.StopPointFlagTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmGeomBuilder.setStopPointFlag(WedmGeomBuilder.StopPointFlagTypes stopPointFlag)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.