Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmGeomBuilder.SmoothLeadInTypes |
WedmGeomBuilder.SmoothLeadInTypes.NONE
smooth leadin type none
|
static WedmGeomBuilder.SmoothLeadInTypes |
WedmGeomBuilder.SmoothLeadInTypes.SPECIFY
smooth leadin type specify
|
Modifier and Type | Method and Description |
---|---|
WedmGeomBuilder.SmoothLeadInTypes |
WedmGeomBuilder.smoothLeadInOption()
Returns the Smooth Leadin Flag
License requirements: cam_base ("CAM BASE") . |
static WedmGeomBuilder.SmoothLeadInTypes |
WedmGeomBuilder.SmoothLeadInTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmGeomBuilder.SmoothLeadInTypes |
WedmGeomBuilder.SmoothLeadInTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmGeomBuilder.SmoothLeadInTypes[] |
WedmGeomBuilder.SmoothLeadInTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmGeomBuilder.setSmoothLeadInOption(WedmGeomBuilder.SmoothLeadInTypes leadInFlag)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.