Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static WedmArcOutputTypeCiBuilder.OutputTypes |
WedmArcOutputTypeCiBuilder.OutputTypes.CIR_PERP_TO_TAXIS
cir perp to taxis
|
static WedmArcOutputTypeCiBuilder.OutputTypes |
WedmArcOutputTypeCiBuilder.OutputTypes.LINEAR_ONLY
linear only
|
Modifier and Type | Method and Description |
---|---|
WedmArcOutputTypeCiBuilder.OutputTypes |
WedmArcOutputTypeCiBuilder.outputType()
Returns the Motion Output Type
License requirements: None. |
static WedmArcOutputTypeCiBuilder.OutputTypes |
WedmArcOutputTypeCiBuilder.OutputTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WedmArcOutputTypeCiBuilder.OutputTypes |
WedmArcOutputTypeCiBuilder.OutputTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WedmArcOutputTypeCiBuilder.OutputTypes[] |
WedmArcOutputTypeCiBuilder.OutputTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WedmArcOutputTypeCiBuilder.setOutputType(WedmArcOutputTypeCiBuilder.OutputTypes outputType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.