Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
LatheUserDefined
Represents a Lathe User Defined operation
To create or edit an instance of this class, use LatheUserDefinedBuilder Created in NX7.5.0 |
interface |
MillUserDefined
Represents a Mill User Defined operation
To create or edit an instance of this class, use MillUserDefinedBuilder Created in NX7.5.0 |
interface |
WedmUserDefined
Represents a User Defined WEDM operation
To create or edit an instance of this class, use WedmUserDefinedBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
UserDefinedOpr |
UserDefinedOpr.getSourceUdop()
Get source udop for the exit udopcopy
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.