Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.TrackingPointType.AUTO
automatic
|
static TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.TrackingPointType.FIXED
fixed
|
static TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.TrackingPointType.ROTATE
rotate with holder
|
Modifier and Type | Method and Description |
---|---|
TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.trackingPointStatus()
Returns the tracking point status
License requirements: None. |
static TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.TrackingPointType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurningOperationBuilder.TrackingPointType |
TurningOperationBuilder.TrackingPointType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurningOperationBuilder.TrackingPointType[] |
TurningOperationBuilder.TrackingPointType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurningOperationBuilder.setTrackingPointStatus(TurningOperationBuilder.TrackingPointType status)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.