Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.AUTOMATIC
Test Cut Stop Position: Automatic
|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.LENGTH
Test Cut Stop Position: Length
|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.PERCENT
Test Cut Stop Position: Percent of Finish Cut
|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.POINT
Test Cut Stop Position: Point
|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.SAME_AS_FIRST_TEST_CUT
Test Cut Stop Position: Same as First Test Cut
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.stopPosition()
Returns the test cut stop position
License requirements: None. |
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishTestCut.StopPositionTypes |
TurnRoughFinishTestCut.StopPositionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishTestCut.StopPositionTypes[] |
TurnRoughFinishTestCut.StopPositionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishTestCut.setStopPosition(TurnRoughFinishTestCut.StopPositionTypes stopPosition)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.