Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.AXIAL_RADIAL
Test Cut Return Move: Axial -> Radial
|
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.DIRECT
Test Cut Return Move: Direct
|
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.RADIAL_AXIAL
Test Cut Return Move: Radial -> Axial
|
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.SAME_AS_FIRST_TEST_CUT
Test Cut Return Move: Same as First Test Cut
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.returnMoveOption()
Returns the test cut return move
License requirements: None. |
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishTestCut.ReturnMoveTypes |
TurnRoughFinishTestCut.ReturnMoveTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishTestCut.ReturnMoveTypes[] |
TurnRoughFinishTestCut.ReturnMoveTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishTestCut.setReturnMoveOption(TurnRoughFinishTestCut.ReturnMoveTypes returnMove)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.