Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.DISTANCE
Local Return: Distance
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.NONE
Local Return: None
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.NUMBER_OF_CUTS
Local Return: Number of Cuts
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.NUMBER_OF_LEVELS
Local Return: Number of Levels
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.NUMBER_OF_PASSES
Local Return: Number of Passes
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.TIME
Local Return: Time
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.mode()
Returns the local return type
License requirements: None. |
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes |
TurnRoughFinishLocalReturnBuilder.ModeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishLocalReturnBuilder.ModeTypes[] |
TurnRoughFinishLocalReturnBuilder.ModeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishLocalReturnBuilder.setMode(TurnRoughFinishLocalReturnBuilder.ModeTypes localReturnModeType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.