Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.ALIGNMENT
Ajustment: Alignment
|
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.NONE
Ajustment: None
|
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.RANGE
Ajustment: Range
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.adjustmentMode()
Returns the adjustment mode mode
License requirements: None. |
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes[] |
TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishLocalReturnBuilder.setAdjustmentMode(TurnRoughFinishLocalReturnBuilder.AdjustmentModeTypes adjustmentMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.