Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.CORNER_AFTER_WALL
Groove Corner Control cut sequence is Corner After Wall.
|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.CORNER_WITH_WALL
Groove Corner Control cut sequence is Corner With Wall.
|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.CORNERS_FIRST
Groove Corner Control cut sequence is Corners First.
|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.CORNERS_FIRST_AND_LAST
Groove Corner Control cut sequence is Corners First and Last.
|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.CORNERS_LAST
Groove Corner Control cut sequence is Corners Last.
|
Modifier and Type | Method and Description |
---|---|
TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.cutSequence()
Returns the Groove Corner Control cut sequence
License requirements: None. |
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnGrooveCornerControl.CutSequenceTypes |
TurnGrooveCornerControl.CutSequenceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnGrooveCornerControl.CutSequenceTypes[] |
TurnGrooveCornerControl.CutSequenceTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnGrooveCornerControl.setCutSequence(TurnGrooveCornerControl.CutSequenceTypes cutSequence)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.