Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
TurnFeatureGeomBuilder.SurfaceSensitivityModes.DISTANCE
Surface sensitivity is active.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
TurnFeatureGeomBuilder.SurfaceSensitivityModes.NONE
Surface sensitivity is inactive.
|
Modifier and Type | Method and Description |
---|---|
TurnFeatureGeomBuilder.SurfaceSensitivityModes |
TurnFeatureGeomBuilder.surfaceSensitivityMode()
Returns the surface sensitivity mode
License requirements: cam_base ("CAM BASE") . |
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
TurnFeatureGeomBuilder.SurfaceSensitivityModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes |
TurnFeatureGeomBuilder.SurfaceSensitivityModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnFeatureGeomBuilder.SurfaceSensitivityModes[] |
TurnFeatureGeomBuilder.SurfaceSensitivityModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnFeatureGeomBuilder.setSurfaceSensitivityMode(TurnFeatureGeomBuilder.SurfaceSensitivityModes surfaceSensitivityMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.