Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.RadiusOptions.ADD_TO_TOOL_RADIUS
Concave Corner Control radius option is Add to Tool Radius.
|
static TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.RadiusOptions.SPECIFY
Concave Corner Control radius option is Specify.
|
static TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.RadiusOptions.TOOL_RADIUS
Concave Corner Control radius option is Tool Radius.
|
Modifier and Type | Method and Description |
---|---|
TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.radiusOption()
Returns the Concave Corner Control radius option
License requirements: None. |
static TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.RadiusOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnConcaveCornerControl.RadiusOptions |
TurnConcaveCornerControl.RadiusOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnConcaveCornerControl.RadiusOptions[] |
TurnConcaveCornerControl.RadiusOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnConcaveCornerControl.setRadiusOption(TurnConcaveCornerControl.RadiusOptions radiusOption)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.