Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidancePathPointsBuilder.PointStatus |
TurnAvoidancePathPointsBuilder.PointStatus.ACTIVE
Point Status: Active
|
static TurnAvoidancePathPointsBuilder.PointStatus |
TurnAvoidancePathPointsBuilder.PointStatus.INACTIVE
Point Status: Inactive
|
TurnAvoidancePathPointsBuilder.PointStatus |
TurnAvoidancePathPointsBuilder.PointData.pointstatus
the point status
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidancePathPointsBuilder.PointStatus |
TurnAvoidancePathPointsBuilder.PointStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidancePathPointsBuilder.PointStatus |
TurnAvoidancePathPointsBuilder.PointStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidancePathPointsBuilder.PointStatus[] |
TurnAvoidancePathPointsBuilder.PointStatus.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidancePathPointsBuilder.modifyData(int index,
NXObject specifyPoint,
TurnAvoidancePathPointsBuilder.MotionTypes motionType,
TurnAvoidancePathPointsBuilder.FeedrateModesTypes feedrateType,
double customFeedrateValue,
TurnAvoidancePathPointsBuilder.CustomFeedrateUnitTypes customFeedrateUnit,
TurnAvoidancePathPointsBuilder.PointStatus pointStatus,
int startEventFlag,
NXObject startEventPath,
int endEventFlag,
NXObject endEventPath)
Modify an existing avoidance path point,name maybe changed if not unique
License requirements: cam_base ("CAM BASE") . |
void |
TurnAvoidancePathPointsBuilder.setPointData(int index,
NXObject specifyPoint,
TurnAvoidancePathPointsBuilder.MotionTypes motionType,
TurnAvoidancePathPointsBuilder.FeedrateModesTypes feedrateType,
double customFeedrateValue,
TurnAvoidancePathPointsBuilder.CustomFeedrateUnitTypes customFeedrateUnit,
TurnAvoidancePathPointsBuilder.PointStatus pointStatus,
int startEventFlag,
NXObject startEventPath,
int endEventFlag,
NXObject endEventPath)
Create a new avoidance path point, name maybe changed if not unique.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.