Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
TurnAvoidanceGohomeBuilder.GohomePointModes.POINT
Point is defined by point.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
TurnAvoidanceGohomeBuilder.GohomePointModes.SAME_AS_FROM
Point is locked to from point.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceGohomeBuilder.GohomePointModes |
TurnAvoidanceGohomeBuilder.gohomePointMode()
Returns the gohome point mode
License requirements: None. |
static TurnAvoidanceGohomeBuilder.GohomePointModes |
TurnAvoidanceGohomeBuilder.GohomePointModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
TurnAvoidanceGohomeBuilder.GohomePointModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes[] |
TurnAvoidanceGohomeBuilder.GohomePointModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceGohomeBuilder.setGohomePointMode(TurnAvoidanceGohomeBuilder.GohomePointModes gohomePointMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.