Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.NONE
Path is inactive.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.POINTS
Path is defined by points.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.POINTS_BEFORE_TOOL_CHANGE
Path is defined by points, but applied only before tool change.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.SAME_AS_APPROACH
Path is locked to approach path.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.SAME_AS_APPROACH_BEFORE_TOOL_CHANGE
Path is locked to approach path, but applied only before tool change.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.departurePathMode()
Returns the departure path mode
License requirements: None. |
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes |
TurnAvoidanceDepartureBuilder.DeparturePathModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceDepartureBuilder.DeparturePathModes[] |
TurnAvoidanceDepartureBuilder.DeparturePathModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceDepartureBuilder.setDeparturePathMode(TurnAvoidanceDepartureBuilder.DeparturePathModes departurePathMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.