Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.ApproachPathModes.NONE
Path is inactive.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.ApproachPathModes.POINTS
Path is defined by points.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.ApproachPathModes.POINTS_AFTER_TOOL_CHANGE
Path is defined by points, but applied only after tool change.
|
Modifier and Type | Method and Description |
---|---|
TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.approachPathMode()
Returns the approach path mode
License requirements: None. |
static TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.ApproachPathModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes |
TurnAvoidanceApproachBuilder.ApproachPathModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceApproachBuilder.ApproachPathModes[] |
TurnAvoidanceApproachBuilder.ApproachPathModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnAvoidanceApproachBuilder.setApproachPathMode(TurnAvoidanceApproachBuilder.ApproachPathModes approachPathMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.