Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TrimPoint.Options |
TrimPoint.Options.NONE
Point is inactive.
|
static TrimPoint.Options |
TrimPoint.Options.POINT
Point is active.
|
Modifier and Type | Method and Description |
---|---|
TrimPoint.Options |
TrimPoint.option()
Returns the trim point option
License requirements: None. |
static TrimPoint.Options |
TrimPoint.Options.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimPoint.Options |
TrimPoint.Options.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimPoint.Options[] |
TrimPoint.Options.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimPoint.setOption(TrimPoint.Options trimPointMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.