Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TrimPoint.AngleOptions |
TrimPoint.AngleOptions.ANGLE
Angle is defined by a value.
|
static TrimPoint.AngleOptions |
TrimPoint.AngleOptions.AUTO
Angle is calculated automatically.
|
static TrimPoint.AngleOptions |
TrimPoint.AngleOptions.VECTOR
Angle is defined by a vector.
|
Modifier and Type | Method and Description |
---|---|
TrimPoint.AngleOptions |
TrimPoint.angleOption()
Returns the trim point angle option
License requirements: None. |
static TrimPoint.AngleOptions |
TrimPoint.AngleOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimPoint.AngleOptions |
TrimPoint.AngleOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimPoint.AngleOptions[] |
TrimPoint.AngleOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimPoint.setAngleOption(TrimPoint.AngleOptions angleMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.