Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ToolAxisVariable.NominalLeadAngleTypes |
ToolAxisVariable.NominalLeadAngleTypes.NONE
None
|
static ToolAxisVariable.NominalLeadAngleTypes |
ToolAxisVariable.NominalLeadAngleTypes.SPECIFY
Specify
|
Modifier and Type | Method and Description |
---|---|
ToolAxisVariable.NominalLeadAngleTypes |
ToolAxisVariable.nominalLeadAngleType()
Returns the Nominal Lead Angle type
License requirements: None. |
static ToolAxisVariable.NominalLeadAngleTypes |
ToolAxisVariable.NominalLeadAngleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ToolAxisVariable.NominalLeadAngleTypes |
ToolAxisVariable.NominalLeadAngleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ToolAxisVariable.NominalLeadAngleTypes[] |
ToolAxisVariable.NominalLeadAngleTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ToolAxisVariable.setNominalLeadAngleType(ToolAxisVariable.NominalLeadAngleTypes nominalLeadAngle)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.