Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
ThreadedBossSet |
HoleBossGeom.createThreadedBossBuilder(NXObject[] entities,
double diameter,
double height,
NXObject toolAxis,
double majorDiameter,
double minorDiameter,
double lengh,
String size,
double pitch,
int rotation,
HoleBossGeom.FormTypes form,
String formUserDefined)
Create a new Thread Boss
License requirements: cam_base ("CAM BASE") . |
ThreadedBossSet |
ThreadedBossSetList.findItem(int index)
Returns the object at the input index.
|
ThreadedBossSet[] |
ThreadedBossSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ThreadedBossSetList.append(ThreadedBossSet object)
Appends an object to the list
License requirements: None. |
void |
ThreadedBossSetList.append(ThreadedBossSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ThreadedBossSetList.erase(ThreadedBossSet obj)
Erases the object from the list, but does not delete the object.
|
void |
ThreadedBossSetList.erase(ThreadedBossSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ThreadedBossSetList.findIndex(ThreadedBossSet obj)
Finds the index where the input object appears.
|
void |
ThreadedBossSetList.insert(int location,
ThreadedBossSet object)
Inserts an object at the specified location
License requirements: None. |
void |
ThreadedBossSetList.setContents(ThreadedBossSet[] objects)
Sets the contents of the entire list.
|
void |
ThreadedBossSetList.swap(ThreadedBossSet object1,
ThreadedBossSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.