Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.CHECK
Use selected check geometry
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.CONTOUR_POSITION
Use end point of last contouring
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.DRIVE
Use drive geometry start or stop point
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.POINT
Use selected point
|
Modifier and Type | Method and Description |
---|---|
TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.startPositionMethod()
Returns the start position method
License requirements: None. |
TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.stopPositionMethod()
Returns the stop position method
License requirements: None. |
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TeachmodeProfileMoveBuilder.StartStopPositionMethods[] |
TeachmodeProfileMoveBuilder.StartStopPositionMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TeachmodeProfileMoveBuilder.setStartPositionMethod(TeachmodeProfileMoveBuilder.StartStopPositionMethods newValue)
License requirements: cam_base ("CAM BASE") . |
void |
TeachmodeProfileMoveBuilder.setStopPositionMethod(TeachmodeProfileMoveBuilder.StartStopPositionMethods newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.