Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TabPointDataBuilder.TabMethodType |
TabPointDataBuilder.TabMethodType.POINT_AND_WIDTH
Point and Width
|
static TabPointDataBuilder.TabMethodType |
TabPointDataBuilder.TabMethodType.START_AND_END_POINT
Start and End point
|
Modifier and Type | Method and Description |
---|---|
TabPointDataBuilder.TabMethodType |
TabPointDataBuilder.tabMethod()
Returns the tab method option
License requirements: cam_base ("CAM BASE") . |
static TabPointDataBuilder.TabMethodType |
TabPointDataBuilder.TabMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TabPointDataBuilder.TabMethodType |
TabPointDataBuilder.TabMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TabPointDataBuilder.TabMethodType[] |
TabPointDataBuilder.TabMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TabPointDataBuilder.setTabMethod(TabPointDataBuilder.TabMethodType method)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.