Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static RoughTurningBuilder.PartOffPositionModeTypes |
RoughTurningBuilder.PartOffPositionModeTypes.AUTOMATIC
Part Off Position Mode: Automatic
|
static RoughTurningBuilder.PartOffPositionModeTypes |
RoughTurningBuilder.PartOffPositionModeTypes.SPECIFY
Part Off Position Mode: Specify
|
Modifier and Type | Method and Description |
---|---|
RoughTurningBuilder.PartOffPositionModeTypes |
RoughTurningBuilder.partOffPositionMode()
Returns the Part Off Position Mode
License requirements: None. |
static RoughTurningBuilder.PartOffPositionModeTypes |
RoughTurningBuilder.PartOffPositionModeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoughTurningBuilder.PartOffPositionModeTypes |
RoughTurningBuilder.PartOffPositionModeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoughTurningBuilder.PartOffPositionModeTypes[] |
RoughTurningBuilder.PartOffPositionModeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoughTurningBuilder.setPartOffPositionMode(RoughTurningBuilder.PartOffPositionModeTypes partOffPositionMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.