Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static RoughFinishTurningBuilder.RegionMachiningTypes |
RoughFinishTurningBuilder.RegionMachiningTypes.MULTIPLE
Region Machining type: Multiple
|
static RoughFinishTurningBuilder.RegionMachiningTypes |
RoughFinishTurningBuilder.RegionMachiningTypes.SINGLE
Region Machining type: Single
|
Modifier and Type | Method and Description |
---|---|
RoughFinishTurningBuilder.RegionMachiningTypes |
RoughFinishTurningBuilder.regionMachining()
Returns the Region Machining type
License requirements: None. |
static RoughFinishTurningBuilder.RegionMachiningTypes |
RoughFinishTurningBuilder.RegionMachiningTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoughFinishTurningBuilder.RegionMachiningTypes |
RoughFinishTurningBuilder.RegionMachiningTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoughFinishTurningBuilder.RegionMachiningTypes[] |
RoughFinishTurningBuilder.RegionMachiningTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoughFinishTurningBuilder.setRegionMachining(RoughFinishTurningBuilder.RegionMachiningTypes regionMachining)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.