Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.AXIAL_RADIAL
axial and then radial
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.AXIAL_RADIAL_WITH_CLEARANCE
axial and then radial from/to clearance
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.CLEARANCE
from/to clearance
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.DIRECT
direct
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.NONE
none
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.RADIAL_AXIAL
radial and then axial
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.RADIAL_AXIAL_WITH_CLEARANCE
radial and then axial from/to clearance
|
Modifier and Type | Method and Description |
---|---|
ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.approachFlag()
Returns the approach from clearance plane flag
License requirements: None. |
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProbeProtectedParametersBuilder.AppMethodTypes |
ProbeProtectedParametersBuilder.AppMethodTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProbeProtectedParametersBuilder.AppMethodTypes[] |
ProbeProtectedParametersBuilder.AppMethodTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProbeProtectedParametersBuilder.setApproachFlag(ProbeProtectedParametersBuilder.AppMethodTypes approachFrom)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.