Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ProbeInspectSurfacePointMoveBuilder.Direction |
ProbeInspectSurfacePointMoveBuilder.Direction.NORMAL
Inferred using surface normal
|
static ProbeInspectSurfacePointMoveBuilder.Direction |
ProbeInspectSurfacePointMoveBuilder.Direction.VECTOR
Specify vector
|
Modifier and Type | Method and Description |
---|---|
ProbeInspectSurfacePointMoveBuilder.Direction |
ProbeInspectSurfacePointMoveBuilder.directionType()
Returns the direction type
License requirements: None. |
static ProbeInspectSurfacePointMoveBuilder.Direction |
ProbeInspectSurfacePointMoveBuilder.Direction.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProbeInspectSurfacePointMoveBuilder.Direction |
ProbeInspectSurfacePointMoveBuilder.Direction.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProbeInspectSurfacePointMoveBuilder.Direction[] |
ProbeInspectSurfacePointMoveBuilder.Direction.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProbeInspectSurfacePointMoveBuilder.setDirectionType(ProbeInspectSurfacePointMoveBuilder.Direction dirType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.