Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static PitchSetting.VarianceTypes |
PitchSetting.VarianceTypes.CONSTANT
Constant
|
static PitchSetting.VarianceTypes |
PitchSetting.VarianceTypes.START_AND_END
Start and End
|
static PitchSetting.VarianceTypes |
PitchSetting.VarianceTypes.START_AND_INCREMENT
Start and Increment
|
Modifier and Type | Method and Description |
---|---|
static PitchSetting.VarianceTypes |
PitchSetting.VarianceTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PitchSetting.VarianceTypes |
PitchSetting.VarianceTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PitchSetting.VarianceTypes[] |
PitchSetting.VarianceTypes.values()
Returns an array that contains the values for this enum.
|
PitchSetting.VarianceTypes |
PitchSetting.variance()
Returns the pitch variance
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
PitchSetting.setVariance(PitchSetting.VarianceTypes pitchVariance)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.