Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OperationBuilder.OptimizationLevelTypes |
OperationBuilder.OptimizationLevelTypes.ADVANCED
advanced
|
static OperationBuilder.OptimizationLevelTypes |
OperationBuilder.OptimizationLevelTypes.STANDARD
standard
|
Modifier and Type | Method and Description |
---|---|
OperationBuilder.OptimizationLevelTypes |
OperationBuilder.optimizationLevel()
Returns the optimization level in operation
License requirements: None. |
static OperationBuilder.OptimizationLevelTypes |
OperationBuilder.OptimizationLevelTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationBuilder.OptimizationLevelTypes |
OperationBuilder.OptimizationLevelTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationBuilder.OptimizationLevelTypes[] |
OperationBuilder.OptimizationLevelTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OperationBuilder.setOptimizationLevel(OperationBuilder.OptimizationLevelTypes optimType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.