Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static OperationBuilder.HoleAxisTypes |
OperationBuilder.HoleAxisTypes.RULE
Rule
|
static OperationBuilder.HoleAxisTypes |
OperationBuilder.HoleAxisTypes.RULE_IF_NO_VECTOR
Rule if no vector
|
static OperationBuilder.HoleAxisTypes |
OperationBuilder.HoleAxisTypes.VECTOR
Vector
|
Modifier and Type | Method and Description |
---|---|
OperationBuilder.HoleAxisTypes |
OperationBuilder.holeAxisType()
Returns the Hole Axis Type
License requirements: None. |
static OperationBuilder.HoleAxisTypes |
OperationBuilder.HoleAxisTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OperationBuilder.HoleAxisTypes |
OperationBuilder.HoleAxisTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OperationBuilder.HoleAxisTypes[] |
OperationBuilder.HoleAxisTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
OperationBuilder.setHoleAxisType(OperationBuilder.HoleAxisTypes types)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.