Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.GlobalStopPointTypes |
NcmWedmBuilder.GlobalStopPointTypes.OPSTOP
stop points option opstop
|
static NcmWedmBuilder.GlobalStopPointTypes |
NcmWedmBuilder.GlobalStopPointTypes.STOP
stop points option stop
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.GlobalStopPointTypes |
NcmWedmBuilder.globalStopPointType()
Returns the global_stop_point_type
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.GlobalStopPointTypes |
NcmWedmBuilder.GlobalStopPointTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.GlobalStopPointTypes |
NcmWedmBuilder.GlobalStopPointTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.GlobalStopPointTypes[] |
NcmWedmBuilder.GlobalStopPointTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setGlobalStopPointType(NcmWedmBuilder.GlobalStopPointTypes globalStopPointType)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.