Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.SmoothToleranceSources.CUTTING
use cutting tolerance type
|
static NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.SmoothToleranceSources.MINIMIZE_POINTS
minimize points tolerance type
|
static NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.SmoothToleranceSources.SPECIFY
specify tolerance type
|
Modifier and Type | Method and Description |
---|---|
NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.engRetToleranceSource()
Returns the engage/retract tolerance source
License requirements: None. |
NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.transferToleranceSource()
Returns the transfer/rapid tolerance type
License requirements: None. |
static NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.SmoothToleranceSources.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmSmoothingBuilder.SmoothToleranceSources |
NcmSmoothingBuilder.SmoothToleranceSources.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmSmoothingBuilder.SmoothToleranceSources[] |
NcmSmoothingBuilder.SmoothToleranceSources.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmSmoothingBuilder.setEngRetToleranceSource(NcmSmoothingBuilder.SmoothToleranceSources newValue)
License requirements: cam_base ("CAM BASE") . |
void |
NcmSmoothingBuilder.setTransferToleranceSource(NcmSmoothingBuilder.SmoothToleranceSources newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.