Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.MeasureHeightFrom.CURRENT_LEVEL
Measure from current level
|
static NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.MeasureHeightFrom.PLANE
Measure from user-defined plane
|
static NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.MeasureHeightFrom.PREVIOUS_LEVEL
Measure from previous level
|
Modifier and Type | Method and Description |
---|---|
NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.heightFrom()
Returns the height from which engage helical/ramp/plunge is measured
License requirements: None. |
static NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.MeasureHeightFrom.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmPlanarEngRetBuilder.MeasureHeightFrom |
NcmPlanarEngRetBuilder.MeasureHeightFrom.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmPlanarEngRetBuilder.MeasureHeightFrom[] |
NcmPlanarEngRetBuilder.MeasureHeightFrom.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmPlanarEngRetBuilder.setHeightFrom(NcmPlanarEngRetBuilder.MeasureHeightFrom newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.