Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.NO_POINT
use no point (only for GoHome point)
|
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.NONE
Avoidance point inactive
|
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.USE_OTHER
use from point (only for GoHome point)
|
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.USE_POINT
use specified point
|
Modifier and Type | Method and Description |
---|---|
NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.pointStatus()
Returns the point status
License requirements: None. |
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmAvoidancePointBuilder.PointStates |
NcmAvoidancePointBuilder.PointStates.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmAvoidancePointBuilder.PointStates[] |
NcmAvoidancePointBuilder.PointStates.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmAvoidancePointBuilder.setPointStatus(NcmAvoidancePointBuilder.PointStates newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.