Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static LaserProfileMove.InterpMethods |
LaserProfileMove.InterpMethods.CUBIC_SPLINE
Cubic Spline
|
static LaserProfileMove.InterpMethods |
LaserProfileMove.InterpMethods.LINEAR
Linear
|
static LaserProfileMove.InterpMethods |
LaserProfileMove.InterpMethods.SMOOTH
Smooth
|
Modifier and Type | Method and Description |
---|---|
LaserProfileMove.InterpMethods |
LaserProfileMove.interpMethod()
Returns the Interpolation Method
License requirements: None. |
static LaserProfileMove.InterpMethods |
LaserProfileMove.InterpMethods.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaserProfileMove.InterpMethods |
LaserProfileMove.InterpMethods.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaserProfileMove.InterpMethods[] |
LaserProfileMove.InterpMethods.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaserProfileMove.setInterpMethod(LaserProfileMove.InterpMethods type)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.