Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
LaserControlPoint |
LaserProfileMove.createControlPoint(int headOrientType,
Point pointTag,
CartesianCoordinateSystem csysTag,
int processType,
boolean toggle,
NXObject udePathTag,
int pointType)
Create a new Laser Control Point
License requirements: cam_base ("CAM BASE") . |
LaserControlPoint |
LaserControlPointList.findItem(int index)
Returns the object at the input index.
|
LaserControlPoint[] |
LaserControlPointList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LaserControlPointList.append(LaserControlPoint object)
Appends an object to the list
License requirements: None. |
void |
LaserControlPointList.append(LaserControlPoint[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
LaserControlPointList.erase(LaserControlPoint obj)
Erases the object from the list, but does not delete the object.
|
void |
LaserControlPointList.erase(LaserControlPoint obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
LaserControlPointList.findIndex(LaserControlPoint obj)
Finds the index where the input object appears.
|
void |
LaserControlPointList.insert(int location,
LaserControlPoint object)
Inserts an object at the specified location
License requirements: None. |
void |
LaserControlPointList.setContents(LaserControlPoint[] objects)
Sets the contents of the entire list.
|
void |
LaserControlPointList.swap(LaserControlPoint object1,
LaserControlPoint object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.