Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static LaserControlPoint.ProcessTypes |
LaserControlPoint.ProcessTypes.DRIVE_TO_POINT
Drive to Point
|
static LaserControlPoint.ProcessTypes |
LaserControlPoint.ProcessTypes.PROJECT_TO_TOOL_PATH
Project to Tool Path
|
Modifier and Type | Method and Description |
---|---|
LaserControlPoint.ProcessTypes |
LaserControlPoint.processType()
Returns the Point Process Type
License requirements: None. |
static LaserControlPoint.ProcessTypes |
LaserControlPoint.ProcessTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LaserControlPoint.ProcessTypes |
LaserControlPoint.ProcessTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LaserControlPoint.ProcessTypes[] |
LaserControlPoint.ProcessTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LaserControlPoint.setProcessType(LaserControlPoint.ProcessTypes type)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.