Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
IpwContainmentCurvesBuilder.ThicknessModeValue.DISTANCE
use thickness mode distance
|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
IpwContainmentCurvesBuilder.ThicknessModeValue.POINT
use thickness mode point
|
Modifier and Type | Method and Description |
---|---|
IpwContainmentCurvesBuilder.ThicknessModeValue |
IpwContainmentCurvesBuilder.thicknessMode()
Returns the thickness mode
License requirements: None. |
static IpwContainmentCurvesBuilder.ThicknessModeValue |
IpwContainmentCurvesBuilder.ThicknessModeValue.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IpwContainmentCurvesBuilder.ThicknessModeValue |
IpwContainmentCurvesBuilder.ThicknessModeValue.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IpwContainmentCurvesBuilder.ThicknessModeValue[] |
IpwContainmentCurvesBuilder.ThicknessModeValue.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IpwContainmentCurvesBuilder.setThicknessMode(IpwContainmentCurvesBuilder.ThicknessModeValue method)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.