Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static IpwAnalysisBuilder.ColorControl |
IpwAnalysisBuilder.ColorControl.BLEND
use sharp color control
|
static IpwAnalysisBuilder.ColorControl |
IpwAnalysisBuilder.ColorControl.SHARP
use blend color control
|
Modifier and Type | Method and Description |
---|---|
IpwAnalysisBuilder.ColorControl |
IpwAnalysisBuilder.colorControlType()
Returns the control color
License requirements: None. |
static IpwAnalysisBuilder.ColorControl |
IpwAnalysisBuilder.ColorControl.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IpwAnalysisBuilder.ColorControl |
IpwAnalysisBuilder.ColorControl.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IpwAnalysisBuilder.ColorControl[] |
IpwAnalysisBuilder.ColorControl.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IpwAnalysisBuilder.setColorControlType(IpwAnalysisBuilder.ColorControl type)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.