Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionMeasDataBuilder.BoundingType |
InspectionMeasDataBuilder.BoundingType.BOUNDED |
static InspectionMeasDataBuilder.BoundingType |
InspectionMeasDataBuilder.BoundingType.UNBOUNDED |
Modifier and Type | Method and Description |
---|---|
InspectionMeasDataBuilder.BoundingType |
InspectionMeasDataBuilder.holePinMatching()
Returns the hole pin matching mode when adding measured data
License requirements: None. |
static InspectionMeasDataBuilder.BoundingType |
InspectionMeasDataBuilder.BoundingType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionMeasDataBuilder.BoundingType |
InspectionMeasDataBuilder.BoundingType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionMeasDataBuilder.BoundingType[] |
InspectionMeasDataBuilder.BoundingType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionMeasDataBuilder.setHolePinMatching(InspectionMeasDataBuilder.BoundingType holePinMatching)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.