Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.PointTypeEnums.DELTA_XYZ
Enter in a delta value from a point
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.PointTypeEnums.EXISTING_POINT
Select an existing point
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.PointTypeEnums.POINT_CONSTRUCTOR
Use the Point Constructor
|
Modifier and Type | Method and Description |
---|---|
InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.pointTypeEnum()
Returns the point type enum
License requirements: None. |
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.PointTypeEnums.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
InspectionLinearMoveToPointBuilder.PointTypeEnums.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums[] |
InspectionLinearMoveToPointBuilder.PointTypeEnums.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionLinearMoveToPointBuilder.setPointTypeEnum(InspectionLinearMoveToPointBuilder.PointTypeEnums pointTypeEnum)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.