Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
InPathEventDataBuilder |
WedmCustomBoundaryDataBuilder.createInpathEventDataBuilder()
The create inpath event data builder
License requirements: cam_base ("CAM BASE") . |
InPathEventDataBuilder |
InPathEventDataBuilderList.findItem(int index)
Returns the object at the input index.
|
InPathEventDataBuilder[] |
InPathEventDataBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
InPathEventDataBuilderList.append(InPathEventDataBuilder object)
Appends an object to the list
License requirements: None. |
void |
InPathEventDataBuilderList.append(InPathEventDataBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
InPathEventDataBuilderList.erase(InPathEventDataBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
InPathEventDataBuilderList.erase(InPathEventDataBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
InPathEventDataBuilderList.findIndex(InPathEventDataBuilder obj)
Finds the index where the input object appears.
|
void |
InPathEventDataBuilderList.insert(int location,
InPathEventDataBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
InPathEventDataBuilderList.setContents(InPathEventDataBuilder[] objects)
Sets the contents of the entire list.
|
void |
InPathEventDataBuilderList.swap(InPathEventDataBuilder object1,
InPathEventDataBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.