Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static HoleBossGeom.RotationTypes |
HoleBossGeom.RotationTypes.LEFT_HAND
Rotation: Left-hand
|
static HoleBossGeom.RotationTypes |
HoleBossGeom.RotationTypes.RIGHT_HAND
Rotation: Right-hand
|
Modifier and Type | Method and Description |
---|---|
HoleBossGeom.RotationTypes |
HoleBossGeom.rotation()
Returns the Rotation types
License requirements: None. |
static HoleBossGeom.RotationTypes |
HoleBossGeom.RotationTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HoleBossGeom.RotationTypes |
HoleBossGeom.RotationTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HoleBossGeom.RotationTypes[] |
HoleBossGeom.RotationTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HoleBossGeom.setRotation(HoleBossGeom.RotationTypes type)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.