Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
HoldingSystemBuilder |
HoldingSystemBuilderList.findItem(int index)
Returns the object at the input index.
|
HoldingSystemBuilder[] |
HoldingSystemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
HoldingSystemBuilderList.append(HoldingSystemBuilder object)
Appends an object to the list
License requirements: None. |
void |
HoldingSystemBuilderList.append(HoldingSystemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
HoldingSystemBuilderList.erase(HoldingSystemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
HoldingSystemBuilderList.erase(HoldingSystemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
HoldingSystemBuilderList.findIndex(HoldingSystemBuilder obj)
Finds the index where the input object appears.
|
void |
HoldingSystemBuilderList.insert(int location,
HoldingSystemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
HoldingSystemBuilderList.setContents(HoldingSystemBuilder[] objects)
Sets the contents of the entire list.
|
void |
HoldingSystemBuilderList.swap(HoldingSystemBuilder object1,
HoldingSystemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.