Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Method and Description |
---|---|
DriveChainItemBuilder |
DmCurveBuilder.createDpmcvDriveCurve(Section section)
Create a Drive Curve
License requirements: cam_base ("CAM BASE") . |
DriveChainItemBuilder |
DriveChainItemBuilderList.findItem(int index)
Returns the object at the input index.
|
DriveChainItemBuilder[] |
DriveChainItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DriveChainItemBuilderList.append(DriveChainItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
DriveChainItemBuilderList.append(DriveChainItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
DriveChainItemBuilderList.erase(DriveChainItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
DriveChainItemBuilderList.erase(DriveChainItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
DriveChainItemBuilderList.findIndex(DriveChainItemBuilder obj)
Finds the index where the input object appears.
|
void |
DriveChainItemBuilderList.insert(int location,
DriveChainItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
DriveChainItemBuilderList.setContents(DriveChainItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
DriveChainItemBuilderList.swap(DriveChainItemBuilder object1,
DriveChainItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.