Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CutParametersIpwTypes |
CutParametersIpwTypes.LEVEL_BASED
level based type
|
static CutParametersIpwTypes |
CutParametersIpwTypes.LOCAL
Local to feature
|
static CutParametersIpwTypes |
CutParametersIpwTypes.NONE
none
|
static CutParametersIpwTypes |
CutParametersIpwTypes.THICKNESS
Thickness
|
static CutParametersIpwTypes |
CutParametersIpwTypes.THREE_DIMENSION
3d type
|
static CutParametersIpwTypes |
CutParametersIpwTypes.TWO_DIMENSION
2d type
|
static CutParametersIpwTypes |
CutParametersIpwTypes.USE_REFERENCE_TOOL
Use reference tool
|
Modifier and Type | Method and Description |
---|---|
CutParametersIpwTypes |
CutParameters.ipwType()
Returns the IPW type
License requirements: None. |
static CutParametersIpwTypes |
CutParametersIpwTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CutParametersIpwTypes |
CutParametersIpwTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CutParametersIpwTypes[] |
CutParametersIpwTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CutParameters.setIpwType(CutParametersIpwTypes propValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.