Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CutParametersFilletsTypes |
CutParametersFilletsTypes.ADD_INTO_DIAMETERS
Fillets mode: Add into Diameters
|
static CutParametersFilletsTypes |
CutParametersFilletsTypes.ADD_INTO_FACES
Fillets mode: Add into Faces
|
static CutParametersFilletsTypes |
CutParametersFilletsTypes.OMIT
Fillets mode: Omit
|
static CutParametersFilletsTypes |
CutParametersFilletsTypes.SPLIT
Fillets mode: Split
|
Modifier and Type | Method and Description |
---|---|
CutParametersFilletsTypes |
TurnCutParameters.cutFillets()
Returns the fillets mode
License requirements: None. |
static CutParametersFilletsTypes |
CutParametersFilletsTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CutParametersFilletsTypes |
CutParametersFilletsTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CutParametersFilletsTypes[] |
CutParametersFilletsTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnCutParameters.setCutFillets(CutParametersFilletsTypes filletsMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.