Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CutParametersExtendAtStartMode |
CutParametersExtendAtStartMode.INCLUDE_ADJACENT_CHAMFERS_OR_ROUNDS
Include Adjacent Chamfers or Rounds
|
static CutParametersExtendAtStartMode |
CutParametersExtendAtStartMode.NONE
None
|
static CutParametersExtendAtStartMode |
CutParametersExtendAtStartMode.TO_CONTAINMENT_GEOMETRY
To Containment Geometry
|
Modifier and Type | Method and Description |
---|---|
CutParametersExtendAtStartMode |
TurnCutParameters.extendAtStart()
Returns the Corner Start Extension
License requirements: None. |
static CutParametersExtendAtStartMode |
CutParametersExtendAtStartMode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CutParametersExtendAtStartMode |
CutParametersExtendAtStartMode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CutParametersExtendAtStartMode[] |
CutParametersExtendAtStartMode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnCutParameters.setExtendAtStart(CutParametersExtendAtStartMode mode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.